SUG_Wiser-00

Manage Users

The Manage Users menu allows you to add new users and grant them access to devices or actions linked with your Wiser account.

The Manage Users feature includes two options:

  • Owned: This option grants full access to the devices. As the owner, you can manage all settings, add or remove devices, and make necessary changes.

  • Shared: This option grants limited access to the devices. Shared users can control the devices but cannot add or remove them. They can interact with the devices based on the permissions set by the owner, such as adjusting settings or viewing status updates.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?