Adding a Device
-
The Wiser Hub must be installed before adding a Wiser device.
-
The instructions provided for adding the device are generic. Some steps may vary based on the device types. You can find detailed information in the Device User Guide of the respective device. Refer to List of Wiser Devices for the links to Device user guide for each devices.
- On the Home screen, tap
Devices.
The Device Management screen appears. - Tap Devices > +.The Add Device screen appears.
- Tap Preferred > With Hub > Type of Device (A).
- Enter the following Device Information and then tap Next:
-
Enter Device Name: Enter the device name.
-
Assign Existing Room: Select an existing room.
TIP: If your room is not in the existing room list, create a new one. -
Add New Room: Create a new room.
-
- Tap Next and choose one of the following
options to pair the device with the Wiser Hub.
-
Press the pairing button once and make sure that the LED blinks green.
Wait for a few seconds until the LED turns green.
TIP: If the LED is blinking red, then the device is not paired to the Hub. Reset the device and start pairing again. -
Press the toggle Switch-1 3 times (Sequence: ON-OFF ON-OFF ON-OFF) within 4 seconds.
NOTE: If the relay puck is installed inside the wall box, the status LED is not visible.
-
- After a few minutes, you can see the Wiser message. Tap Ok.You can see the newly added device on the Device Management screen under Devices.
You can now control the Device with the Wiser App. You can find detailed information about controlling your Devices in chapter Controlling the Wiser System