Energy
|
Energy Monitoring Device 1 Phase ENMOD1P |
The Energy Monitoring Devices is used to monitor the power consumption of the connected loads. |
Wi-Fi® (Communication protocol) |
|
|
Energy Monitoring Device 3 Phase ENMOD3P |
The Energy Monitoring Devices is used to monitor the power consumption of the connected loads. |
Wi-Fi® (Communication protocol) |
|
|
Acti9 Active AFDD A9TDNC606 A9TDNC610 A9TDNC616 A9TDNC625 A9TDNC632 A9TDNC640 A9TDND606 A9TDND610 A9TDND616 A9TDND620 A9TDND625 A9TDND632 |
Arc fault detection devices (AFDD) offer enhanced safety for homes and buildings. AFDD mitigates the risk of electrical fires caused by electrical arcs resulting from faulty or worn electrical appliances and circuits. Thus, AFDD immediately trips as soon as it detects a potentially dangerous arc. It is tolerant of electrical arcs caused by the normal operation of electrical devices such as switches, brushed motors and the plugging and unplugging of devices. |
Z-Wave (Communication protocol) |