SUG_Wiser-00

Notifications and Alarm

Notifications and Alarm allow you to view messages related to your connected devices, keep informed about their status and activities, and see devices added or deleted from the Wiser System.
  1. On the Home screen, tap .
  2. Tap Alarm to see the device messages, such as added or deleted from the Wiser System.
    IMPORTANT: You must enable the Notify Me button from the Profile menu to receive the messages and alarms of the devices.
  3. Tap Notifications to see the device notifications, such as device offline or online.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?