SUG_Wiser-00

Updating Firmware

You can update the firmware of all devices using the Wiser app.

Firmware updates are intended for security and functional updates to help ensure that the System is always up to date. The firmware updates automatically and it runs in the background.

  1. On the Home screen, tap .
  2. Tap Update Firmware.
  3. Tap Update All or Update for individual devices.
After sometime, you will see the Update Firmware status message.

If any device fails to update, tap Retry.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?