SUG_Wiser-00

Selecting the Mounting Location

The Wiser Hub is the controller of the system and must be within a range of all devices in order for the system to work properly.

The ideal location for the Wiser Hub is determined by the following:

  • Layout of the building where the system is installed.

  • Location of other devices that will be used in the system.

General Instructions for Hub and Device Mounting

Referring to the diagram, it is most important to install the Hub (A) as central as possible to the area occupied by all mains-powered devices (B), such as switches, dimmers, shutters, and fan controllers.

Energy Monitoring Device Mounting Requirements

The Wiser Hub (A) is recommended to be installed within 3 meters of Energy Monitoring Devices (B) to ensure strong connection.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?