SUG_Wiser-00

Changing the Wiser Hub Wi-Fi® Access Point

You can change the Wiser Hub Wi-Fi® network using the Wiser app.
IMPORTANT: Change Access point is not allowed when the Hub is setup with Ethernet and online.
  1. On the Home screen, tap Devices > Devices.
  2. Select Wiser Hub.
  3. On the top-right screen, tap .
  4. Tap Change Access Point (A) to change the Wi-Fi® network.
    The Select Wi-Fi page appears.
  5. Select the Wi-Fi® network which you want to connect.
    TIP: If you can’t find your Wi-Fi® network, try tapping Refresh (B). If you still cannot find it, you can manually enter the SSID by tapping Enter SSID (C).
  6. Enter the new Wi-Fi® password in the password field (D).
  7. Tap Connect.
    Wait for a few minutes, you can see the successful Wiser pop-up message.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?