SUG_Wiser-00

Updating the Hub Firmware

Firmware updates are intended for security and functional updates to help ensure that the System is always up to date. The firmware updates automatically and it runs in the background.

You can also update the firmware manually by using the Wiser App.

To update the firmware:

  1. On the Home screen, tap Devices > Devices.
  2. Select the Hub.
    The About Hub screen appears.
  3. On the Device Control Screen, tap .
    The Hub Settings screen appears.
  4. Tap Update Hub Firmware (A).
  5. Enter the Wiser App password and tap Continue.
It will take a few minutes to update the firmware. Once the update is completed, you will see a successful pop-up message.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?