SUG_Wiser-00

Connecting Devices to the Wiser Hub

For the Wiser devices to be controlled by the Hub, they must be connected to the Hub.

Connecting devices to the Hub is part of the setup process. You can add devices to the Wiser Hub at any time. The app guides you through the process of adding devices.

You can find detailed information about the necessary steps for adding the device in the chapter Adding a Device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?