About Wiser Hub
The Multi Protocol Gateway (hereafter referred to as the Wiser Hub), a versatile communication interface designed to connect with all your Zigbee and Z-Wave devices. This Wiser Hub allows you to effortlessly manage and control your home environment.
Functions:
-
Monitors and controls Zigbee and Z-wave devices via the Wiser app with Ethernet or Wi-Fi®.
-
Allows you to create Actions or Automations to operate Zigbee and Z-Wave devices using the Wiser app.
On the Home screen, tap Devices > Devices and select the Hub to access the Device Control Screen.
The Device Control Screen displays the following options:
| A |
Hub Name |
Displays the Hub name. |
| B |
Hub Status |
Displays the Hub status (Offline/Online). |
| C |
Power |
Displays the power connection. |
| D |
Room |
Displays the room name. |
| E |
Internet (Wi-Fi®/Ethernet) |
Displays the Hub connectivity with Wi-Fi® or Ethernet.
NOTE: The Wi-Fi® signal strength can only be seen
when you set up the Wiser Hub with Wi-Fi®.
|
| F |
Hub Information |
Displays the Hub type, ID, Firmware version, and IP address. |
| G |
Time |
Displays the plugged-in time and up time. |
| H |
Connected Devices |
Displays the connected devices, tap to view the connected devices. |
| J |
Settings |
Tap to view the Hub settings. Refer Hub settings for more information. |