SUG_Wiser-00

Editing a Schedule

You can edit a schedule using the Wiser app.
  1. On the Home screen, tap Devices > Devices.
  2. Select Wi-Fi® devices for which you want to edit a schedule.
  3. On the Device Control screen, tap Schedule.
  4. Tap Schedule, select the schedule you want to edit, and then tap .
  5. On the Update Schedule screen, you can perform the following actions:
    • Tap to update the name of the schedule.

    • Tap ON time and OFF time to update the scheduled time.

    • Adjust the control options such as brightness percentage, fan speed, or shutter percentage.

    • In the Perform on section, add or remove the days you want to update.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?