SUG_Wiser-00

Device Control

You can control a Device in your Home directly on the Device Management screen for quick control or in the Device Control Screen.

Devices

On the Devices tab, you can find all the devices installed in your home. The devices are arranged according to the Rooms they are assigned to, making it easy to manage and control them.

  1. On the Home screen, tap Devices > Devices.

  2. Tap on the icon (A) available on each device to quickly control a device (e.g., turn it ON/FF and adjust the shutter).

NOTE: (B) indicates that the device is offline. Tap on the device to open the troubleshooting steps. Scroll up to see more details about the Z-Wave signal strength. Tap Contact support if you require further assistance and visit our Wiser Support Pages.

Device Control Screen

The advanced controls such as device settings or creating/assigning actions will be performed in the Device Control Screen.

  1. On the Home screen, tap Devices > Devices.

  2. Select the device which you want to access the Device Control Screen.

A

Power Button

Allows you to change the status of the device ON/OFF.

B

Schedule

Allows you to create quick actions and trigger automations.

C

History

Allows you to see the history of the device. Tap to update the history of the device when you open the History screen.

D

Settings

Allows you to control various settings. For more information, refer to the Configuring the device topic of the respective device user guide.

E

Favourites

Allows you to add the device to the favourites on the Home screen.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?