Setting up the Wiser Hub with Ethernet
Before setting up the Wiser System, you need to create an account. Refer to creating an account.
Before setting up the Wiser Hub with Ethernet, connect the Ethernet cable to the Wiser Hub. Also, connect your mobile device to the Wi-Fi® network.
To set up the Wiser System:
- Login to the Wiser App.
- On the Home screen, tap
Devices.
- Tap Devices > +.The Add Device screen appears.
- Tap Preferred > With
Hub >
Wiser Hub.
The Wiser Hub screen appears. - Enter the following Hub information:
- Tap Ethernet (D).
- Connect the Ethernet cable to the Wiser Hub, and then tap Next.
- Check the status of the Ethernet LED indicator and select Solid Green from the following options (E):
-
Solid Green: Indicates an internet connection.
-
Blinking Green: Indicates no internet connection.
-
- Tap Next.The Wiser pop-up appears.
- Tap Ok and scan either of the two
QR codes located behind the Wiser Hub or on the packing box.Wait for a few minutes, and you will see the successful setup screen. You can see the newly added Hub on the Device Management screen under Devices.