Setting up the Wiser Hub with Bluetooth
To set up the Wiser System:
- Login to the Wiser App.
- On the Home screen, tap
Devices.
- Tap Devices > +.The Add Device screen appears.
- Tap Preferred > With
Hub >
Wiser Hub.
The Wiser Hub screen appears. - Enter the following Hub information:
- Tap Bluetooth (D).
- Select the check box of Confirm that the LED
is blinking RED and, then tap Start Configuration.TIP: If the LED is solid red or blinking slowly, then reset the device. For more information, refer to the Resetting the device topic.
- Turn On your phone’s Bluetooth or tap Allow to enable Bluetooth.
- After a few seconds, you can see the Wiser Hub details.
Select Wiser Hub.TIP: If you are unable to find the device name, tap Search Again.
- When the Bluetooth pairing request message appears, tap Pair.
- Select your home Wi-Fi® network and enter
the password, and then tap Confirm.TIP: If you are unable to find the Wi-Fi® network, tap Enter SSID to connect manually. Tap Refresh to update the Wi-Fi® list.