SUG_Wiser-00

Setting up the Wiser Hub

In order to be able to control the system via your smartphone, the Wiser Hub must be connected to the internet.

You can set up the Wiser Hub by using the Wiser app.

You can setup the Wiser System by using the app after creating an account. Refer to Setting up an Account for information on how to create an account.

You can set up the Wiser System using the following options:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?