SUG_Wiser-00

Updating Wi-Fi® Network

You can update the Wi-Fi® network using the Wiser app.
  1. On the Home screen, tap .
  2. Tap Update Wi-Fi.
    The Update Wi-Fi pop-up appears.
  3. Enable your phone's Bluetooth. and make sure that your phone is in near to the devices.
    After sometime, you can see all Bluetooth paired devices.
    TIP: If you do not see all devices, tap Scan Again to find all devices.
  4. Select all or individual devices for which you want to change the Wi-Fi® network.
  5. Tap Connect to Wi-Fi.
  6. Select your home Wi-Fi® network, enter your password, and then tap Confirm.
After sometime, you will see the Connected message on the screen. Also, you can see the Status message.

If any device connection fails, tap Try Again to update.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?