SUG_Wiser-00

Deleting a Room

You can delete a room using the Wiser app.

To delete:

  1. On the Home screen, tap Devices > Rooms.
  2. On the top-right screen, tap .
    The Edit Rooms screen appears.
  3. Tap on the room that you want to remove from the Wiser system.
    NOTE: You cannot delete a room directly if it contains devices. First, remove the devices from the room, then delete the room.
  4. Tap Confirm.
    TIP: You can also delete a room by selecting a room > > Delete Room.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?