SUG_Wiser-00

Energy

In the Energy Center, you can monitor your power grid in real-time, daily, over the last 7 days, monthly, and yearly. You can also access a detailed history of your grid and information on energy savings.

It provides detailed information on the annual bill.

NOTE: This energy data will only be populated if you have the EMD device commissioned with the Wiser System. Otherwise, you will not be able to see any energy-related data.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?