SUG_Wiser-00

Adding a New Location

You can add a new location from the Location menu.
  1. On the Home screen, tap Location .
  2. Tap + Add Location.
  3. On the Add Location screen, enter a new location name.
  4. Tap Add.
    NOTE: Alternatively, you can also create a new location from the Location menu > Location Settings > +.
    TIP: If you want to switch to another location, tap the Location menu and select the location you want to switch.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?