SUG_Wiser-00

LED Behaviour

LED Description

Wi-Fi® LED Blinks

Wi-Fi® signal or internet is not working.

Ethernet LED Blinks

The Ethernet is connected but there is no internet.

Wi-Fi® LED Blinks

The Wi-Fi® is connected but there is no internet.

Wi-Fi® LED Solid

Setting up the Wiser Hub with Wi-Fi®.

Ethernet LED Solid

Setting up the Wiser Hub with Ethernet.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?