SUG_Wiser-00

Schedule

The schedule feature allows you to define the specific time for changing the state of the device.

For example, you can set a specific ON time and OFF time for the light so that the light will be turned ON/OFF at the specific times you choose.

You can also create multiple schedules as per your needs, such as daily routines or special events.

NOTE: This feature is only available in Wi-Fi® devices.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?