Device Settings
You can find all relevant settings of a Device on the Device Settings screen.
You can navigate to the Device Settings from the List of Devices by tapping settings on the Device Control Screen.
|
A |
Device Name |
Displays the device name, tap |
|
B |
Change Room |
Displays the assigned room of the device, tap Change Room to assign any room (such as living room, bedroom, kitchen, etc.). For more information, refer to the respective Device User Guide. |
|
C |
Radio Type |
Displays the Z-Wave network. |
|
D |
Device Type |
Displays the device type. |
|
E |
Signal Strength |
Displays the signal strength. For more information, refer to the About Signal Strength topic. |
|
F |
Advanced Settings |
Allows you to set group switches and configuration. When you tap Advanced Settings, you can see the following options:
|
|
G |
Product Details |
Displays the product details such as manufacturer name, ID, product name, ID, and type. Also you can view the firmware version and update it if a new version is available by tapping Product Details > Firmware Version & OTA. |
|
H |
Notification |
Enable the Notify Me toggle button to receive device notifications. |
Some devices have specific features and settings. For example, Shutter devices have an option to select the shutter type and set the duration for opening and closing. You can find detailed information in the Device User Guide of the respective device. Refer to List of Wiser Devices for the link to device user guide of each devices.