SUG_Wiser-00

Appliances

16A 1M Connected Switch

CS16A1MSW

The 16A 1M Connected Switch is used to operate resistive, inductive or capacitive loads.

Wi-Fi® (Communication protocol)

Instruction Sheet (PDF)

Device User Guide

IR Controller 1Module

CCIRC1M

The IR Controller 1Module is used to automate IR controlled devices such as television, air conditioner, music system and so on.

Wi-Fi® (Communication protocol)

Instruction Sheet (PDF)

Device User Guide

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?