Assign Crew

Available in Responder Explorer.

You can assign work crews to incidents by dragging them from the Crews window to an incident. You can also drag an incident from the Incidents tab to a crew in the Crews window. Crews can be assigned to individual components of an incident using the same methods (e.g., fault device, location feature, hazard).

A crew may appear grayed out in the Crews tab. This indicates a Status of Unavailable or Meal Break (or no status at all). Change their Status to Available to enable the crew for assignment.

The cursor symbol shown below indicates that the crew can be assigned to the present location.

The cursor symbol shown below indicates that the crew cannot be assigned to the present location.

The incident's status changes to Assigned and the crew is listed as Assigned under the incident. The Status field in the Crew Assignments section reflects the current crew status. The Incident icon in the Crews tab also changes color to reflect the crew status. The crew name (in the Crews flyout window) appears in bold when it has been assigned to an incident.

A crew can be assigned to a specific device, location feature, or hazard, or to the incident as a whole. In the example below, crews BC506 and GF5816 are assigned to incident 6179. Crew BC506 has been assigned specifically to XFR229 and the faulty support structure. Crew GF5816 has been assigned to XFR5 and the hazard (ID 165) on that same transformer.

In the graphic below, you can see that the Crew Status also displays at the incident level.

 

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?