Add Switching Operation

Available in Responder Explorer.

This tool is available in the right-click menu on an incident in Responder Explorer.

  1. Right-click a confirmed incident and select Add Switching Operation.
  2. In ArcMap, the cursor becomes a circle with a blue dot that snaps to features. Use this to select the feature for the Switching Operations.
  3. The Add Switching Operation dialog allows the operator to provide an outage time and the name of the person who operated the device.
  4. You can modify the Planned Status. This field lists the phases and phase combinations that can be operated on the device. If the device's normal status is closed, the Planned field shows which phases can be opened. If the device's normal status is opened, the Planned field shows which phases can be closed.
  5. Click OK.

    A switching operation symbol is placed on the feature in the map and a confirmed incident with restoration steps is created in Responder Explorer. Use an Edit tool to modify the restoration steps in Responder Explorer.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?