Main Menu
Available in Responder Explorer.
The main menu is visible at the top of the Switching Order form and contains three categories.
The icon next to the switching order name indicates whether you've opened a switching order or a template. In the above example, the user has a switching order open. If you have a template open, the icon looks like this:
Next to the Order number is the switch order status (e.g., Created, In Execution). The switch order status can be one of the following:
-
Created: No operations in the switch order have been executed.
-
In Execution: Some operations in the switch order have been executed, but not all.
-
Executed: All operations in the switch order have been executed.
The following statuses are visible only if you have the Approval functionality enabled (i.e., the Approval menu is visible in the Main menu on the Switch Order Editor).
-
Pending Approval: This status indicates that a switch order has been submitted for approval. Only a user with approval permissions can open and approve this switch order.
-
Approval Denied: This status indicates that a switch order has been rejected by an approval officer.
-
Approved: This status indicates that a switch order has been approved and can now be executed.