Complete Hazard

Available in Responder Explorer.

Responder allows the user to specify a hazard as completed.

  1. Right-click a hazard (regardless of its secured status) and select Complete.
  2. Provide information about the hazard on the Complete Hazard form.
  3. Click OK.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?