Unpopulated Fields

If a fault is placed at the fuse or a downstream device, Responder is unable to populate the FeederID and Substation fields because it cannot determine which feeder—F1, F2, or F3—has the fault. In this situation, the fields are left blank. One way to access this information is via a comma-delimited list, available in:  

Responder Line Display.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?