Analytical

This tab displays several types of information in the form of graphs. The information shown is for the region selected on the left.

  • Customer Status: The percentage reflects the amount of customers affected by any type of incident.

  • Interruption Status: The percentage reflects the number of interruptions with no crew assigned.

  • Crew Status: This data displays the total number of crews and the percentage assigned to incidents and hazards.

  • Hazards Status: This data displays the number of hazards and the percentage assigned to crews.

  • Call Status: This portion displays the status of incoming calls, such as the number of active calls and the number that have not been restored within 30 minutes.

  • Outage Cost: Displays the dollar amount of revenue lost due to the current outages.

  • Estimated Time of Restoration: Displays the estimated time of restoration for the selected region. This reflects the estimated time of restoration set on the Restoration Estimates page in the Dispatchers section.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?