Modify Snippet

  1. Add the snippet to a switching order (if it has not already been added to one).
  2. Modify the operations as needed.
  3. Select all operations to be included, and then right-click the snippet and select Save/Modify Snippet.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?