Incident Filters
Available in Responder Explorer.
The Incidents tab allows you to use filters to display incidents. Select a filter from the drop-down menu to change the display. The selected filter also takes into account the setting of the Show Regions toggle button. If it is set to Show All Regions, the filter applies to all regions. If it is set to Show My Regions, the filter applies only to the regions that are assigned to the current user. To the left of the filter field you can see which Show Regions setting is in effect (‘All Incidents in My Regions’ in the example below).
The plus/minus buttons at the top-left corner of the tab allow you to easily expand (+) all displayed incidents in the grid or contract them (-).
The default filters for Responder Explorer are listed below. Filters can be customized, so the filters in your Responder Explorer may be different.
-
Table-Field: Allows the user to perform a query on the Incidents table. In the example below, the filter is set to display all incidents that have the value ‘No Power’ in the Call Trouble field.
-
For 10.8.1 and later only
Table-Multifield: Allows you to apply filters for multiple fields at once and displays results that match all selected filters.
To apply multiple filters, click Add Row then select the Field and Value for each filter you want to search on.

-
All: Displays all incidents.
-
My Incidents: Displays all incidents assigned to the current user.
-
Critical: Displays only incidents with critical customers.
-
Active: Displays only incidents that have not been completed or closed.
-
Complete: Displays only incidents that have been completed, but not yet closed.
-
Min. Customer Count: Displays incidents that affect the number of customers equal to or greater than the number provided. In the example below, Responder is set to locate any incidents that affect 42 or more customers.
-
No Crew Assigned: Displays all incidents that have not had crews assigned to them. Incidents that have a status of Restored, but do not have a crew assigned to them, are filtered out of the display.
-
No Crew Working: Displays all incidents on which crews are not working. This filter includes incidents that have had crews dispatched to them, but the crews are not yet working, along with incidents that have not yet had crews assigned to them.
-
No Owner: Displays all incidents that have a value of <Unassigned> in the Owner field.
-
Outage Time > 8 hours: Displays all incidents that have an outage time of greater than eight hours.
-
Incidents without switch order: Displays all incidents that have no switching orders assigned.
-
Incidents with switch order(s): Displays all incidents that DO have switching orders assigned.
-
Network Level: There is no separate filter for network level groupings. If you have configured your geodatabase to use Network Level groupings, use the Table-Field filter to query this field.