Remove Jumper in ArcMap

Available in ArcMap.

An operator can manually remove a jumper on the map. Responder removes the jumper from the corresponding incident in Responder Explorer. If the jumper is the only child record of the incident, the entire incident is canceled.

Responder Explorer must be open to remove a jumper in ArcMap.

  1. In ArcMap, locate the jumper on the map.
  2. Click the Remove Jumper button on the Responder toolbar. The cursor becomes a circle with a blue dot in the middle. The blue dot snaps to selectable electric line features with the proper model name assigned. A layer must be set as selectable before this tool can snap to its features.
  3. Click the jumper line feature to remove.
    A confirmation message to remove the jumper appears.
  4. Click Yes.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?