Dispatchers Tab

Available in Responder Explorer.

The Dispatchers tab displays all dispatchers that have access to the regions currently displayed as well as all incidents assigned to those dispatchers. Expand the plus sign next to a dispatcher's name to view the assigned incidents.

The only right-click tool available on this tab is when you select an incident. You can right-click it and select Show Incident in Grid.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?