Edit Hazard

Available in Responder Explorer.

You can edit the hazards associated with an incident on the Incidents tab. Access the Edit Hazard form by right-clicking a hazard under an incident.

  1. Right-click a hazard and select Edit.
  2. The Edit Hazard dialog displays information about the selected hazard.
  3. You can edit the following information about the hazard: type, wire owner, remarks, and public safety information.

    The Public Safety section indicates the arrival time of public safety officials at the scene (e.g., fire, police) and when they leave.

  4. Click OK to save changes and dismiss the dialog.

    Click the Set to Now button to set the field to the current date and time.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?