Switching Order Details

The right side of the screen displays details about the selected switching order or template. The switching order details can be edited only when you open the switching order or template in the Switching Order Editor. The window includes the following three tools:

  • Open: This tool opens the selected switching order or template.

  • Display on Map: This tool is enabled only if you have ArcMap open. Select Display on Map to view the switch order devices and outage area in ArcMap. The device(s) are highlighted on the map with a callout. When you close the Switching Order Library, the callout on the map is removed.

  • Delete: Click this button to delete the currently selected switching order or template. You are then prompted to confirm deletion of the selected object.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?