Remove Tag

Available in ArcMap and Responder Explorer.
This tool allows you to remove existing tags. Follow these steps to remove tags:
  1. Click the Remove Tag button on the Responder toolbar.

    The cursor becomes a circle with a blue dot in the middle. The blue dot snaps to all selectable devices. A layer must be set as selectable before this tool snaps to its features.

  2. Select a device with a tag to display the Remove Tag dialog.
  3. In the Remove Tag dialog display, click OK to remove the tag.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?