Select Regions

Available in Responder Explorer.

Responder provides various Select Region tools. Responder also provides the ability to create regions and group them into one or two parent regions. The Select Regions tools allow you to select either individual region polygons or a region group. By default, only the Select Regions tool is available in Responder.

Select Regions

Displays a list of your assigned regions. You can select the regions to view. This also changes your region assignment. For example, if you select the Boyne City checkbox in the image below, you are a dispatcher to that region and can create incidents in Boyne City.

The next two tools are not available in Responder Explorer unless your administrator adds them to the user interface. See the Responder Configuration Guide for more information.

Select Parent Region 1*

Provides a dialog to select the parent regions to be viewed in Responder Explorer. The regions in this list have the RXREGIONPARENT1 model name assigned.

Select Parent Region 2*

Provides a dialog to select the parent regions to be viewed in Responder Explorer. The regions in this list have the RXREGIONPARENT2 model name assigned.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?