Edit Switching/Restoration Order

Available in Responder Explorer.

There are multiple ways to open and edit an existing switching order, restoration order, or template.

NOTE: You can select the Refresh Device States option from the Order menu (or press F5) to update the actual state of all devices in all open switching and restoration orders. This is useful when a change is being made to a device while the Switching Order Editor window is still open.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?