Crews

Available in Responder Explorer.

Responder Explorer allows the dispatcher to create and manage crews and assign them to incidents. A dispatcher can create a crew that has crew member, truck, and radio assignments. This crew can then be assigned to an incident. As the crew reports back to the dispatcher, she can edit the crew's status accordingly. This provides other dispatchers with an accurate picture of what's happening at the incident site.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?