Edit Non-Electric Device

Available in Responder Explorer.

You can edit the non-electric devices (e.g., poles) associated with an incident on the Incidents tab. Access the Edit Location Feature form by right-clicking a non-electric device. Non-electric devices are also referred to as location features.

  1. Right-click a non-electric device and select Edit.
    The Edit Location Feature dialog displays information about the selected feature.
  2. Edit the following information about the feature as needed:
    • Time of Report

      NOTE: Click the Set to Now button to set the field to the current date and time.
    • Confirmed (only if the device has not been confirmed)

    • Remarks

  3. Click OK to save changes and close the dialog.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?