Delete Crew

Available in Responder Explorer.

Responder allows users to delete crews that have no incidents assigned to them. A crew cannot be deleted if it’s assigned to an incident.

  1. Right-click the crew that you want to delete. Delete is available only for crews that do not have any incidents assigned. Crews that are assigned to incidents are displayed in bold.
  2. Select Delete.
  3. Click Yes in the confirmation screen to delete. Click Cancel to cancel deletion of the crew.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?