Insert New Auto Change Time

  1. Next to the Is Auto Change Enabled? field, click List.
    This expands the fields necessary to create a new Auto Change time.
  2. Select a Mode from the drop-down menu.
  3. Provide a Start Time for the mode to become enabled.
  4. Click Insert.
    The Status field displays the status of the operation.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?