Remove Jumper
Available in Responder Explorer.
You can remove jumpers associated with an incident on the Incidents tab.
- Right-click a jumper and select Remove Jumper(s). A confirmation message appears.
- Click Yes to remove the jumper from the incident.
Removing a jumper indicates that the jumper was removed in the field (at the current time). To indicate that a jumper never existed in the field, cancel the incident to which the jumper is assigned.
Scenario A:
-
An outage occurs at 10:00 PM.
-
A jumper is placed to temporarily restore power to the loadpoints in Responder Explorer at 11:00 PM.
Current time of outage: 1 hour.
-
The crew repairs the outage at 1:00 AM, and the dispatcher restores the incident in Responder Explorer at 1:00 AM.
-
The jumper is 'removed' at 1:00 AM in the field and in Responder Explorer.
Total time of outage: 1 hour.
NOTE: A removed jumper is archived. In addition, if you close an incident with an existing jumper, the effect on the jumper is the same as a 'removal' of the jumper at the time of close.
Scenario B:
-
An outage occurs at 10:00 PM.
-
A jumper is placed accidentally in Responder Explorer at 11:00 PM.
Current time of outage: 1 hour.
-
The jumper is 'canceled' at 1:00 AM, because the crew indicated they did not use a jumper. The loadpoints revert to having an outage at the original outage time.
-
The crew repairs the outage, and the dispatcher restores the incident in Responder Explorer at 1:00 AM.
Total time of outage: 3 hours.
NOTE: Jumpers that are part of a canceled incident are not archived (unless all canceled incidents are archived as configured by your administrator).