Available Operations
The following operations are available by default in Responder Web Browser. They can be assigned to tasks as needed.
|
Operation |
Description |
|---|---|
|
APPROVE_SWITCHING_ORDER |
This operation allows users to approve a switch order. |
|
ARCHIVE_MASS_EDIT |
This operation allows users to edit multiple loadpoints or calls of an archived incident at one time. |
|
ARCHIVE_REPORTS |
This operation allows users to run Archive Reports on the Web. |
|
CALL_ALLOW_EDIT_TIME_OF_OUTAGE |
This operation allows users to edit the time of call on the web page (if configured to do so). |
|
CANCEL_SW_OR_REQUESTS |
This operation allows users to cancel switch order requests that they do not own. |
|
CHANGE_NORMAL_STATE |
This operation allows users to use the change normal state tool. |
|
CREATE_SWITCHING_ORDER, DELETE_SWITCHING_ORDER, EDIT_SWITCHING_ORDER |
This operation allows users to create, delete, and edit switch orders. |
|
DELETE_ARCHIVED_INCIDENTS |
This operation allows users to delete incidents, calls, or loadpoints from the Responder Archive Explorer. |
|
DISPATCHER_SELECTABLE |
This operation allows dispatchers to be listed as dispatchers in explorer. |
|
EDIT_SW_OR_REQUESTS |
This operation allows users to edit switch orders that are owned by other users. |
|
EDIT_SWITCHING_ORDER_IN_EXECUTION |
This operation allows users to edit a switch order that is currently in execution. |
|
EXECUTE_SWITCHING_ORDER |
This operation allows users to execute a step on a switch order. |
|
INCIDENT_REVIEW |
This operation allows a user to use the Incident Review tool. |
|
LINE_DISPLAY_REPROCESS_ALL |
This operation allows users to remove and reprocess the current line display and jumpers in ArcMap. NOTE: With this permission you can reprocess the line display
and jumpers for all incidents, regardless of whether you are
the dispatcher for that incident. Without this permission, you can
only reprocess the line display and jumpers for the incidents
in which you are the dispatcher.
|
|
LONG_TERM_DEVICE |
This operation allows users to make a device long term. |
|
MODIFY_FOLDER_STRUCTURE |
This operation allows users to change the folder structure in the library (create, move, delete folders). |
|
MODIFY_TASK_SNIPPETS |
This operation allows users to create/modify snippets. |
|
PLACE_JUMPER |
This operation allows users to place a jumper from ArcMap or within Responder Explorer. |
|
PLAN_SWITCHING_ORDER |
This operation allows users to plan a switch order (setting the start/finish time). |
|
REMOVE_JUMPER |
This operation allows users to remove jumpers from ArcMap and Responder Explorer. |
|
REPROCESS_DEVICES |
This operation allows users to reprocess devices on an incident, updating loadpoints and outage times. |
|
RX_CALLS,DELETE |
This operation is an example of a table-based permission to delete. |
|
RX_CALLS,INSERT |
This operation is an example of a table-based permission to insert. |
|
RX_CALLS,SELECT |
This operation is an example of a table-based permission to select. |
|
RX_CALLS,UPDATE |
This operation is an example of a table-based permission to update. |
|
SAVE_SWITCHING_SIMULATION |
This operation allows users to save switch order simulation results to the database. |
|
SELECTABLE_FOR_EXECUTE_BY |
This operation displays the dispatcher in the dispatcher drop-down for executing steps on a switch order. |