Appendix10.8.1aConfiguration Guide

The Appendix provides lists of ArcFM items such as model names, autoupdaters, and edit tasks. It also offers a description of the Structural Analysis calculations.

The Basic ArcFM Configuration and Basic Designer Configuration pages in the ArcFM Desktop Configuration Guide provide the model names, field model names, and autoupdaters that must be assigned for basic ArcFM and Designer editing functions.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?