GatheringFieldPipe

A gathering field pipe collects gas from the gathering field for distribution.

GASNETWORKEDGE is used to configure gas tracing in ArcFM Viewer for ArcGIS Engine. Assign GASNETWORKEDGE to all Gas Network Edge feature classes that participate in gas tracing.

GatheringFieldPipe acquires properties from the GasPipe abstract class.

Subtypes: None

Associations: None

Model Names: GASNETWORKEDGE

Attributes: None

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?