EmergencyIsolationSystem
The emergency isolation system is used to isolate a portion of the Gas Pressure System in an emergency. It is bound by a critical, normally closed valve. Any GasPipe can participate in only one Emergency Isolation System at a time.
Subtypes: None
Associations: GasPressureSystem
Model Names: None
Attributes:
Field Name |
Field Type |
Description |
---|---|---|
Comments |
text |
User or designer comments. |
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |