NonControllableFitting
Noncontrollable fittings control the flow of natural gas through pipes.
The NONCONTROLFITTING model name, although not required, can be used in gas traces to find all connected equipment belonging to a specific cathodic protection (CP) zone or structure through which current flows to help prevent pipe corrosion.
NonControllableFitting inherits properties from the GasFitting abstract class.
Subtypes: Coupling, Ell, End Cap, Expansion Joint, Flange, Reducer, Tee, Transition
Associations: None
Model Names: NONCONTROLFITTING
Attributes:
Field Name |
Field Type |
Description |
---|---|---|
BondedIndicator |
text |
Indicates whether fitting participates in cathodic protection system; domain values include Yes and No. BondedIndicator uses the BONDEDINDICATOR model name. |