Sectionalizer Unit
Sectionalizers operate in conjunction with breakers and reclosers to lock out fault current after a predetermined number (usually three) of recloser operations (trips).
Designer uses the DESIGNUNIT model name on this class to designate it as an electric device unit object class. The Designer Work Function Tool uses this model name to identify all electric device unit object classes.
Associations: Sectionalizer
Subtypes: None
Model Names: DESIGNUNIT
Attributes:
Field Name |
Field Type |
Description |
---|---|---|
SectionalizerObSjectID |
long integer |
ObjectID of associated Sectionalizer. |
Manufacturer |
text |
Code indicating manufacturer of SectionalizerUnit. |