AbandonedGasDevice

The AbandonedGasDevice feature represents gas devices that have been abandoned in place. It may also contain selected attributes of any gas device, depending on configuration.

Subtypes: None

Associations: None

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

DeviceType

text

Code indicating type of device.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InstallationDate

date

Date of installation.

Manufacturer

text

Code indicating manufacturer. The AT_MANUFACATURER model name is used on this field to configure abandon for gas.

Material

text

Code indicating material of GasDevice. The AT_MATERIAL model name is used on this field to configure abandon for gas.

Model

text

Model number specified by manufacturer. The AT_MODEL model name is used on this field to configure abandon for gas.

PropertyUnitCode

text

Value assigned to assets to track and classify property records.

RetiredDate

date

The date the device was identified as abandoned.

ValveDiameter

text

Diameter of GasValve. The AT_VALVESIZE model name is used on this field to configure abandon for gas.

ValveType

text

Code indicating type of GasValve. The AT_VALVETYPE model name is used on this field to configure abandon for gas.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?